Hi,
I am testing my circuit about bq40z80.
I tried to turn on the CHG mos by CHG_FET_toogle, and Vgs of CHG fet doesn't change, but samely, when using EVM of BQ40z80,I can see Vgs of CHG becomes 10V.
Could I know why?'
Thank you !!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am testing my circuit about bq40z80.
I tried to turn on the CHG mos by CHG_FET_toogle, and Vgs of CHG fet doesn't change, but samely, when using EVM of BQ40z80,I can see Vgs of CHG becomes 10V.
Could I know why?'
Thank you !!
Hi Iris,
Please send the FET_EN command from the command panel. That should turn on the FETs.
Also, please GND the fuse pin.
Hi Batt,
Thany u.
I have tried to use FET_EN, it also didn't work.
The phenomenon is When I send FET_EN, the bit XCHG of OperationStatusA will change from high to low, but the bit CHG keep being low.
Same thing with DSG.
But the cell voltages are all normal.
And I have left the lab, tomorrow I will try to connect fuse to gnd.
Could I know, besides Fuse, are there some other possibilities, and what else directions can I try?
(I want to test whether the problem is about hardware
I'm trying to hope it's not a hardware problem, because pcb cann't be changed.
Thank you very much.
Regards,
Iris
Fuse is the only thing that can toggle FETs off, if your protections and PFs are all clear.
It works after connected fuse to GND.
Thanks!