Dear TI
I read TPS54386/TPS54386-Q1 Datasheet and find a mistake in datasheet!
MSS1278-153ML is 15uH. but Datasheet talk to use 22uH!
Which is it right? 22uH?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI
I read TPS54386/TPS54386-Q1 Datasheet and find a mistake in datasheet!
MSS1278-153ML is 15uH. but Datasheet talk to use 22uH!
Which is it right? 22uH?
Best regards.
Choi,
The circuit does in fact use the 22 uH inductor. The calculated value for L1 and L2 are 18.3 uH and 15.3 uH respectively, based on ripple current of 30%. The conservative approach would be to use the next higher size inductor for lower ac ripple current. In this case 15 uH would still be an appropriate value with slightly higher ripple current.