CSD95372B -Problem: Vin min=4,5v? U LiIon battery=3-4V .Question: Can the CSD95372B work with an input voltage in the range of 3-4v?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CSD95372B -Problem: Vin min=4,5v? U LiIon battery=3-4V .Question: Can the CSD95372B work with an input voltage in the range of 3-4v?
Hi Serg Andre,
Thanks for your interest in the CSD95372B.
This device is not intended for low VIN, high duty cycle applications. That said, as long as you can supply 5V to VDD to power that gate drive and the duty cycle is below the maximum in the datasheet, the part should operate. You may lose some functionality, however. The high-side short detection only operates when VIN is above 3V. The current sense circuit may not meet the accuracy specified in the datasheet.
Best Regards,
Evan