This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940: imon accuracy

Part Number: TPS25940

I would like to use the imon feature at lower current levels, below 100mA, like 10mA.  Can you advise if there are any restrictions on use from 0-100mA and what the linearity and accuracy would be at 10mA-100mA?  Is it still approximately 8% in the low end of the current range?