Part Number: BQ24157
Dear Pros,
We use BQ24157 to set the charge at 1.15a, and the maximum current on the line is only 1.08a。
The charge of the other chip hl7005 is also 1.15a, and the maximum current on the line can reach 1.17a;
Is there a register setting problem?Pls double check。many thanks;
08-14 08:16:03.467222 251 251 D [ 40.179681].(1)[251:charger_thread]: [0x0]=0xd0
08-14 08:16:03.468599 0 0 D [ 40.181058][0x1]: =0xf8
08-14 08:16:03.457762 251 251 I [1565770563.457762].(1)[251:charger_thread]: [0x2]=0xb6
08-14 08:16:03.472996 0 0 D [ 40.185455][0x3]=0x51 .(1)[251: charger_thread][0x4]=0x6a
08-14 08:16:03.473606 0 0 D [ 40.186065][0x5]=0x3 .(1)[251: charger_thread]