Hi!
I have an application where the TPS73225DBVR is fed with very instable input voltages, which could cause the LDO to be switched on and off successively with T<20ms. Vin and EN are tied together.
The first time the input voltage ramps to it's nominal voltage of 3.3V, the LDO outputs correctly its 2.5V as desired.However, with the following switching off and on of the LDO, the full 3.3V Vin is passed to the output for <5ms and then regulated correctly to the 2.5V again.
Do you know this behavior?
What workaround would you propose to prevent the output from exceeding the 2.5V?
Thanks a lot!
Marcus