Part Number: TPS3895
Hi
I use the TPS3895ADRYR as a power on reset signal.
The target voltage= (1+511k/110k)x 0.5= 2.82V.
I know TPS3895A output is push-pull , so I depopulate the R746.
However, I can't see the reset (output) release to high level.
I check the figure 1. of datasheet. It seems that Enable need to be released before Sense.
I measure my EN and Sense which is shown below (P1)
Enable is not released before Sense.
Does the timing of Enable and Sense on P1 cause that output can't be released???
P1