Part Number: TPS7A4001
Linear regulator output dips intermittently and is not periodic. I have 47uF tantalum capacitor @the output which is higher than the min capacitance required for regulation. I have 26V DC input with output voltage of 14V (regulator set) with output current of approximately 23mA, observed the input current and it seems like input current goes to zero intermittently, that tells me that the internal MOSFET is turning off causing momentary dip in linerar regulator output voltage from set level of 14, the dip is not periodic and it looks like exponential decay/rise.
The question I have is why would input current to the linear regulator goes to zero? I measured the part case temperature and is just 30deg c, so thermal limit may not be causing this behaviour.
Could you please help me in understanding why this behaviour is present.