Other Parts Discussed in Thread: DRV8350R,
HI, team,
My customer will use DRV8350R (which integrates LM5008A) and would like to check if the device can support his output power.
The requirement is
- Vin : DC 40 ~ 60V
- Vout : 700mW (=5V*70mA + 3.3V*100mA)
Datasheet explains the current limit is 510mA at Tj=25C. But I would like to know if the 700mW is normal for LM5008A.
Could you please give advice if the device support 700mW output?
Regards,
Nagata