Hi Team,
Could you please help on schematic review for TPS53211?
Thank you.
Best regards,
C.T.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you please help on schematic review for TPS53211?
Thank you.
Best regards,
C.T.
Chentsu,
I have alerted the application support engineer. He is out of the office until Monday. He will review your schematic next week.
8/23/2019
TPS53211 schematic review
How were the R1021, R1025 and C1916, C1914, C1917 were calculated?
The values do not seem to match the design. Typically, the R1021 resistor value is lower than R1022 resistor value.
You can use the equations in the datasheet and the following app note to calculate the value.
Closing the Loop
http://www.ti.com/lit/an/slva301/slva301.pdf
From the schematic, I can not tell how the converter will be layout. The layout of the dc/dc is important, read through PCB layout techniques for best practices.
http://www.ti.com/lit/an/slva963/slva963.pdf
C1902 change to 4.7uF 10V X5R
C1902 ground pad should connect to Pin 15 of 53211
Change C1901 to 2.2uF/10V X5R
C1902 ground pad should connect to Pin 15 of 53211
Add Zero Ohm in series with C1900 Boot capacitor
Change C1913 from 0.22uF to 0.12uF since the inductor is 1.5uH with 1.6mOhm resistance
Regards,
David