Other Parts Discussed in Thread: LM5160
Tool/software: WEBENCH® Design Tools
Hi forum,
i used LM5160ADNTT in its isolated configuration with fly-buck topology.
when i used webench, it was recommend me to choose Cout2 (the capacitor that switch to source during time TON) with the value 270uF, with 5mohm ESR and 5.8A Irms.
the ESR i can understand, the Irms value look over-rated (those two parameters didnt get some attitude on datasheet) and when i used the equation on datasheet to calculate the capacitence i get a value much more lower then the webench recommend me (6uF).
the parameters i was filled on webench are:
- Vin = 8.5-65
- vout = 5 +/- 5%
- Iout = 1.5A
the papameters i was filled in the equation in the datasheets are:
- Iout2 = 1.5A
- (delta)Vout2 = 0.25
- Vout1 = 3.8
- Vin(min) = 8.5
- fsw = 231kHz
it is not make sense and also make me to choose an exotic capacitor (very big and very expensive)
BR,
Itzik