Part Number: UC1825A
Hi,
Question regarding the Clock signal on Pin 4. We use this clock signal to trigger another external circuit. The loading current is about 3.7mA. UC1825A spec has maximum current of 5mA. Is there any issue if we are loading at 3.7mA especially over temperature performance ?
Also, there is a plateau voltage about 0.7V after the pulse turn off. Is this plateau voltage could increase or decrease ?
Best Regards,
Jason