Other Parts Discussed in Thread: LMV431
Hello,
in the Design (http://w*ww.ti.com/lit/df/tidrqf9/tidrqf9.pdf there is T1 (750316708) from Würth.
The truns ratio pri1 to sec is 3:1.
Vin: 12 to 60V.
The secondary winding is defined by 12V. So if 60V is at Vin I get 20V on secondary. Is this a failure?
If I need 48V on the secondary and got 24V on Vin, do I need a ratio of 1:2 for primary winding 1 to secondary winding?
Kind Regards