Hello,
I'm currently testing TPS23758EVM for load , line and ripple performance with output voltage at 5V. I would also like to evaluate the performance at output voltage 3.3V. For this can just changing the resistor divider R19 & R24 suffice .
In datasheet for output voltage setting Raux is also mentioned but I'm unable to correlate the reference designator with the corresponding circuit.