Hi TI-team
The default setting of Vout1 is 1V, but the customer setting is 1.1V, so I want to change it.
From what timing can register be changed ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI-team
The default setting of Vout1 is 1V, but the customer setting is 1.1V, so I want to change it.
From what timing can register be changed ?
Hi, Koji-san,
I've assigned your question to the device expert; please expect to get answer in 24 hours.
Hello Hayashi-san,
You can change the BUCK1_VOUT register (0x0C) data to 0x61 to get 1.1V out from BUCK1. The value can be changed 1.2ms after VANA and NRST are set high. It can be changed when BUCK1 is enabled and running as well.
New data will be in volatile memory, so it will be back to default 1V when device is powered off.
Thanks.
Regards,
Tomi
Hi Tomi-san Phil-san
Thank you for quick response.
I understand that it is best to write to the register before EN = High after applying power.
Is it possible to write a register during soft start of other Bucks ?
Best Regards,
Koji Hayashi
Hello Hayashi-san,
Yes it is possible to write the registers during buck startup. Only requirement is really that the VANA and NRST has been high for 1.2ms to make sure then internal startup (oscillator, OTP read etc) has been completed.
Thanks.
Regards,
Tomi Koskela