Other Parts Discussed in Thread: LM61460, LM73605
Please refer to attached schematic section. We want to control the output voltage from a Microchip MCU through the control of an SPI pot. Although we can set the voltage as expected, the TPS54540 is very unstable except when the digital pot is at it's max or min values. Please let me know if you need a better copy of the schematic and layout. If so, I would like to send those to you directly as opposed to posting them online. I believe that I may need to modify the layout to improve the feedback path with the digital pot.