Other Parts Discussed in Thread: LM36010
Hi:
I want to use TI LM36011 and LM36010. I have the following questions for consultation:
The driving current of flash is 1.5A
1.What is the maximum frame rate?
2.What is the maximum duty ratio at the maximum frame rate?
3.What about the temperature at maximum power consumption?
4.What is the current rise time of the first frame under flash current 1.5a?What is the rise time per frame after that?
5.LM36011&LM36010 Functional difference.