Other Parts Discussed in Thread: UCC38C44
In the datasheet of UC1843B-SP, in page 18/27, Section "Sense Resistor and Slope compensation" it says that when calculating the falling slope of the inductor current (Forward topolofy or buck topology) we have to multiply Vout/L by a gain Gcs=3, here i did not understand from where does this gain come ?? (Equation 46 in the datasheet).
I have gessed that this gain comes from the fact that the output of the Error Amplifier goes through a divider by 3 (Vc is divided by 3 than connected the PWM Comparator).
After a while, i have read the datasheet of UCC38C44 which has the same functional block diagram as UC1843B-SP. In page 13/55 it says "the gain of the current sense amplifier is 3V/V", but when it comes to "slope compensation" section in page 30/55, we do not see the effect of this gain as in UC1843B-SP
Please, can someone clarify this point to me??
How this Gain could affect the ramp compensation design??
What is the effect of the divider of "Error Amplifer output" to the current sense Input ??