Hi,Enginner:
I want ask a question,I used TPS54326 in design and actual work in 1.2V voltage/0.2A current, so the power IC continue to work Eco-mode. if the IC work in Eco-mode for long time is there any problem?like unstability、voltage drop?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Enginner:
I want ask a question,I used TPS54326 in design and actual work in 1.2V voltage/0.2A current, so the power IC continue to work Eco-mode. if the IC work in Eco-mode for long time is there any problem?like unstability、voltage drop?
H,zhao:
if working in Eco-mode Is there any requirement for PWM frequency jitter?In the attachment, there are schematic diagrams and SW test waveforms of 1.5V and 2.5V power supply. Please help to see if there are any problems. thanks.
Best Regards,
shaocong
Hi, Shaocong
As you know, TPS54326 works in Eco-mode at light loading, the operating frequency will change with loading.
So I think the jitter is caused by loading changing, it is correct, no problem.
BTW, the soft start capacitor(1nF) is too small, recommend changing it to 3.3nF which will set soft start time to ~1.26mS.