Other Parts Discussed in Thread: BQ24251EVM-150, BQ24250C
Hi Team,
I would like to evaluate charger + fuel gauge from TI.
In my application I looking for charger with D+/D- so I found BQ24253.
I found that TI doesn't have EVM for BQ24253 only for BQ24251EVM-150, can I use it? is it same die as BQ24253? Does TI recommended this part or other part?
General question – how the D+/D- detection works? It can detect any USB from PC?
I would like to understand how D+/D- detection feature works.
Here are my questions:
- Who is detected between PC USB and charger? Is the PC USB asking which charger is connected or the opposite?
- Who decides how much current will use for the charging? Is it the PC USB based on the handshake with the device?
- If the power source is wall adaptor (connecting to the same USB port on the device) , which current will use for charging?
If there is an application note that describe the handshaking flow it will be excellent.
Thanks,
Shlomi