This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: Query on measuring 30uA using accumulator mode

Part Number: BQ35100


HI,

I want to use BQ35100 for Li-SOCl2 Primary battery of 12Ah for its remaining capacity measurement during operation. Continuous load on the battery is 30uA and hourly or one day once load current goes to 600mA(average) for a few seconds. Do you recommend me to use BQ35100 to know the % of battery capacity remaining?

Is 30uA too small in accumulator mode? And what is the min current can be used in accumulator mode? What is the total error when use the accumulator mode to measure the % of battery capacity remaining?