Hi,
I am planning to use TPS22915B to enter into ship mode for my device. While entering into ship mode (commands sent over USB), I have a condition where the switch is turned off but because I have a USB connected, VOUT pin of TPS22915B still sees a voltage (approx 4.5V). I then remove the USB to go into actual ship mode.
I want to know the maximum current handling capacity of the MOSFET connected between VOUT and GND. Currently I can measure upto 30 mA flowing through it.