Other Parts Discussed in Thread: BQ24610
Hi,
we are using LMZ13610 in our board to 5V conversion.
The input is 12V from adapter or 7.4V from a battery.
BQ24610 is using for power path control and battery charging.
When the battery voltage is around 7.4V, If we remove the AC or connect the AC, the regulator will restart.
Why this is happening?
In the above scenario, we are taking only 3.5A max from the regulator.
Please suggest.
Regards,
Shafeeq