This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTD08D210W: Temperature Sense Output

Part Number: PTD08D210W
Other Parts Discussed in Thread: UCD9248, UCD9220

Hi,

I am using PTD08D210W (dual regulator/module) with power controller UCD9248. Both channels of this module are controlled by 2 rails of UCD9248. However, during monitoring on TI Fusion Digital power designer i observed that temperature readings of both rails were different. Why is this happening?

The PTD08D210W has a single temperature sense output pin which is connected via mux to the temperature sense input of power controller UCD9248. Please see the attached image of schematic for information. Any help regarding the issue will be appreciated.