Tool/software: WEBENCH® Design Tools
Dear All,
I have a problem with a real circuit based on Webench simulation result:
This is 12V-5V DC-DC converter (load current changed from 0 to 1 Amp) - see the attached pictures.
The point is the real circuit shows unexpected and unexplained output voltage ripple (about of 130 mVpp) at light load ( about of 100mA). From second side the ripple at IL=1A seems to me reasonable (about of 20mV pp). No simulation shows this difference.
The electrical circuit has ceramic capacitors only. The bulk capacitance is about of 90uF (not shown on the electrical circuit). The layout done in accordance with your recommendations.
Could you advise please?
Thanks in advance,
Arkadi.