This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563208: Output voltage is not the same as datasheet shows

Part Number: TPS563208

Output is 0.768*(1+R1/R2) according to datasheet, but it outputs more like 0.8*(1+R1/R2)

  • Former Member
    0 Former Member

    Hi Mike,

    Please share me your schematic and test conditions on the measurement of the output.(Vin/Vout/Iout/L/C etc.)

    From the EC table, Vfb of TPS563208 is 0.768V(typ), which is guaranteed by ATE and Correlation test.

    Thanks.