Part Number: UC3842
Hi
We use UC3842D8 to design a 60W/(15V output) power supply. We design the switch frequency is about 100K, but when we test (only 15V output is loaded),the frequency is 20~30Khz, especially 3kHz with no load.
Below is the schematic and some test waveform. I have two question that need to confirm:
1. Is the switch frequency fixed by the RT & CT , anyway different input or load ?
2.Does the schematic need to improve ?