This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61175: Confirming optimal schematic for boost converter

Part Number: TPS61175

Hi there, I wanted to confirm with a specialist that my schematic design is optimal for what I want to do. I used a lot of the information provided from both the datasheet and the TPS61175EVM-326 . My device takes an input voltage of 15V and outputs at 24V. which from the equation for max output current gives me 1.5A. Attached below are the values I have chosen for the passive components to the schematic. Please let me know if you have recommendations for changes or anything. Thanks!