Hi All,
I have designed a PCB using four TPS74801 regulators all running from a 5V input supply. They produce four different output voltages: 1.2, 1.8, 2.5 and 3.3 using the recommended R1/R2 values and output filters shown in the data sheet. Three of the regulator outputs are correct, e.g. within a few percent of their expected values. The 1.8V output however is substantially too high sitting around 2.7V I have measured two boards. One board is 2.68 the other at 2.72 volts. I have removed R1 and R2 from one of these regulator circuits and measured them to be the correct values: 3.57K and 2.87K. The boards are properly cleaned, so flux leakage isn't the issue.
The 1.8V regulator powers a Cypress CX3 CPU, a FSA2466 multiplexer a S25FS128SA serial flash memory and an accelerometer MMA8652FC. I don't see any reverse leakage paths that might be back-feeding the regulator.
Any thoughts most appreciated.
Thanks,
Scott