Hi,
I'm having trouble passing EMC with this FET driver.
The design is for a wireless charger, operating in full-bridge topology using DMT3020 dual FETs.
Operating frequency range is 100-140[kHz.].
It seems as if resistors are required from the driver to the gate of the FET. The values of these resistors are quite high (>20[ohm]). Any way to reduce this value?
Still, there are noises in the following ranges: 20+-5[MHz.], 35+-5[MHz.] & 100+-5[MHz.].
Are there any specific guidelines \ ideas \ tips as to the layout (other than keeping short traces and the usual...)?
Any tips how to reduce emission generated by this driver? I realize that the rest of the circuit is probably radiating as well, but it seems as if the source is coming from the switching done by the driver.
Thanks,
Elieser