Are there any special power sequencing requirements for the TPS51124? I have a system where if the 5 volts comes up before the main supply voltage(12 Volts in this case) the power supply will not turn on, the output voltage stays at 0 volts and the PowerGood signal never asserts itself. If the 12 Volt main supply comes on first followed by the 5 volts then the voltage regulator comes up normally. I am looking through the datasheet but haven't found any specific requirement as to which voltage needs to be active first. Do you have any idea what could be causing the module to not start as expected?