Hello.
I had some questions while was experimenting with BQ79606EVM-897
In the SLEEP mode, the current is specified in the data sheet as 150uA. But when I actually measured (Active --> Go To Sleep command), it was measured at 3.7 mA.
1) What circuits (Comparator, ADC, Communication ...) are enabled so there is a difference of more than 3 mA?
2) What should be done to measure 150uA?
3) If I had to disable the circuit, what circuit would it be?
Thank you.