Other Parts Discussed in Thread: LM34925, , LM5180
Team,
we would like to build an isolated DC/DC power supply:
- Isolated (expected voltage difference between input and output is far below 100 V)
- VIN nominal 48 V (range 40 V - 50 V)
- VOUT 4.0 V, 2.0 A max, max long term output current 1.6 A
- Output overcurrent protection
I found candidates like LM34925 and LM5160A. One concern is that transformer is not from the shelf, but special one (?).
Can you please check requirements and suggest which type would be recommended?
Thank you.