Other Parts Discussed in Thread: , TPS61372
Light load regulation is not so good.
I would like to stabilize the output voltage of at least 10mA.
Is there anything else you'd recommend?
(Condition)
4.2Vin
Setting output voltage is 7.8V.
Output current is up to 200mA.
(Result with electric load device. EVM is TPS61046EVM-682.)
Output current / Output voltage
1mA / 7.892V
10mA / 7.880V
20mA / 7.865V
50mA / 7.808V
100mA / 7.811V
150mA / 7.815V
200mA / 7.819V