This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78020A: Output voltage set-poitn resistor values isssues

Part Number: PTN78020A
Other Parts Discussed in Thread: PTN78020W

Dear whom it may concern,

I am currently analyzing PTN78020WAH to bring 12 V to 5 V. Which I was able to achieve.

However, my Rset value is 13.1 kOhm and it gives 5 V output voltage. By the specification sheet, it is suppose to bring 6 V which is not accepted in our system.

Even though I have a successful output, I just don't understand why.

FYI, I use two parallel 2.2 uF Ceramic in the input voltage, and one 330 uF capacitor on the output. This wouldn't affect that....

Could you please explain how and why this could happen?

Thank you.