Other Parts Discussed in Thread: BQ500212A, BQ500511A, BQ50002A
Tool/software: WEBENCH® Design Tools
Hi,
Can you tell me how found information for calculate the design for the coil Ref :760308102212 ?
Best regards.
Lionel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Lionel
The BQ500210 is an older device without FOD protection circuit. Also is a 19V input and uses an WPC A1 coil with L value of 24uH. Do not recommend changing the coil or power section.
A better device to look at would be the BQ500212A or BQ50002A + BQ500511A. They have FOD, operate from 5V buss and used WPC A5/A11 coil, L=6.3uH.
But due to high circulating currents in the LC tank circuit the DCR of the coil needs to be low.
Hi Johns,
Actually we have BQ5002A+BQ50511A with Coil Ref Wurth : 760308102212 with L=5,4 uH.
On some PCB we realized we have problem a trouble operating the induction.
Or when I put the receiver we can see pulse on SW1 and SW2 and no continuous operation see picture and we can see a variation of the current on power 5V.
Thanks you for u-you answer.
Best regards.
Lionel
Hello Lionel
Working with the BQ5002A+BQ50511A is good, recommend testing with one of the standard WPC A5 / A11 6.3uH coils, Wurth P/N 760 308 105 or 760 308 111.
The Wurth 760308102212 appears to be an RX coil with higher DCR and lower I-SAT.
Hello Johns,
But when I try with 760308102212 it works.
But what I do not understand is why I have 50 PCBs made 13 that does not work. And when I change CI BQ5002+BQ50511A and put the coil 760 308 105 not working. Is strange??
I don't understand.
Thank you for you answer.
Best regards.
Lionel