This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternative to LTC4412

Other Parts Discussed in Thread: TPS2410, LM5050-1

We need a power path controller, which can switch two power sources (12V SMPS Power and 7.4V Li-ion Battery) automatically and also able to detect the presence of the source through controller. For this we are using LTC4412. But currently it is not available in our market and also the price is two high. So, can you please suggest me some IC by TI (power path controller), which can replace LTC4412?

When I contacted to TI for an alternative to LTC4412, they have suggested TPS2314. But, as I have seen, there is no STATUS pin to detect the Power source. You can see that a status pin is available in LTC4412 to detect the power source.So, Can you please suggest me another IC which can do ORing and also can able to detect the power source like LTC4412.