Other Parts Discussed in Thread: LM5118, , , LM5176, LM5170
Tool/software: WEBENCH® Design Tools
Hello,
I am doing a project related with battery charging and discharging. I want to use a bidirectional buck boost DC DC converter for this purpose.
My specifications would be
Lead acid battery 24 V (12 cells of 2 V)
Lithium ion 24 V (8 cells of 3.2 V)
Input voltage= 12 to 26 V. Ranges may vary but nominal voltage is 24 V
Output voltage= 12 to 26 V. Ranges may vary but nominal voltage is 24 V
It should be a bidirectional.
I see an Evaluation board with LM5175 is LM5175EVM-HP and the other controller is LM5118 with LM5118EVM
Now my doubt is whether the boards can be connected in parallel to two different batteries lead acid and lithium ion to increase the capacity. Is it possible to interface with the micro controller because my plan it to control the converter with micro controller such that the converter sends correct amount of voltages to charge the battery and discharge the battery to supply different small DC loads connected to the power supply when power is off.
I already spoke with TI technical support about this. They asked to contact here.