A follow up to- https://e2e.ti.com/support/power-management/f/196/t/846276
Is it possible to provide the list of SBS registers that are cleared and those that are not cleared by the reset command?
The reason I am asking is because there are a number of registers that appear to not be cleared, such as the following:
- Cycle Count
- Max Error
- Registers with failure alerts for failure status
- Operation status register
- Measurement registers: Temperature, Voltage, and Current
Is there a general rule regarding which registers get reset, and which ones do not, when the reset command is issued?