Other Parts Discussed in Thread: TLV431, TL431LI
Hello,
I am using the TLVH431 simulation model in LTspice to evaluate the pulse response specified in datasheet, fig 12 and 13 on page 11 and 12. Despite I use the same circuit as in datasheet, the result is far from datasheet waveform. The reference voltage has large oscillation upon power up. When the rising time of the 3V input is 200ns, the reference oscillates between 3V and 0V. The oscillation dies down after 1.7us. When the rising time is slowed to 600ns, the reference still has some oscillation with larger amplitude and longer duration than the datasheet waveform.
I will trust datasheet over the simulation model for now until I can verify it on a sample. Meanwhile please update the pspice simulation model. Thanks.
Best regards,
Zhenyu