Other Parts Discussed in Thread: TPS63002, TPS63000, TPS63001
We are testing TPS63002 for generating 5V/0.4A output. The input for the circuit is single cell lithium ion battery (3.7V/850mAH). As the input is connected, the output is 0V for both load and without load condition. We checked the enable pin & found it to be high. Also there is no switching taking place on either of the inductors ( L1 / L2 ). We also wired TPS63002 on the evaluation board TPS3000EVM-148. The output was same as mentioned above. Can you suggest cause for the same and how to proceed for obtaining the desired output?
Thanks
Sidhyesh