In the datasheet of LM3466 has no information related to switching characteristics of internal MOSFET.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the datasheet of LM3466 has no information related to switching characteristics of internal MOSFET.
Dear Ramalingam50,
I believe there is some slew rate limiting/ramp control there and I believe is on the order of 10 ms, but will have to investigate further and it will not be something that has been characterized, thus it will not be a guaranteed specification. I also believe the filter on the VEQ lines as well as the filter on the ILED will affect timing.
Is there a specific requirement you need to meet for timing? More information about the application would be helpful along with a schematic. If it is proprietary then we can take this offline.
-fhoude
Prithviraj,
I do not think given the internal slew rate of the LM3466 that it is suitable for your application. In terms of other recommendations, our newer devices are mostly buck or boost/buck-boost type LED drivers or controllers, and TI also has several linear LED drivers.
Feel free to browse further on ti.com
Regards,
Sumeet