Hi,
PIN3 ON, What is the threshold voltage for opening and closing ?
This PIN is externally connected to the control chip, so we want to see whether the specific value of threshold voltage of high and low level matches.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
PIN3 ON, What is the threshold voltage for opening and closing ?
This PIN is externally connected to the control chip, so we want to see whether the specific value of threshold voltage of high and low level matches.
Thanks!
Hi Neal,
Are you referring to the V_IH and V_IL levels?
Assuming the appropriate voltage is on V_in, V_IH is 1V while V_IL is 0.5V.
Note that ON voltage can range to 5V and is not limited by the V_in voltage.