This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82822: alternative for the TPSM82821 that can't be found on the website

Part Number: TPSM82822
Other Parts Discussed in Thread: TPSM82821, , TPS82084

Hello team,

one of my customers is looking to supply a Lattice FPGA that works at 1.1V and 2.5V with roughly 1 A of current. They have available a supply of 3.3V and 5V from which to start and they also noticed that TPSM82821SILR would be a good candidate.

Unfortunately the device is visible on Webench but on the website.

Could you please confirm if it's a valid choice? If yes, can you please let me know the pricing for 1k units?

Thank you and best regards,

Adrian

  • Hi Adrian,

    The TPSM82822 is sampling on the web.  It is pin to pin with the TPSM82821, so you can use TPSM82822 until TPSM82821 is available.

    Both of these devices are pre-release, so please email me with your customer's situation so we can make sure we can meet your needs.

    TPS82084 is a released 2A module that you can ramp with today.