Other Parts Discussed in Thread: BQ78350-R1
Hello,
we are using BQ76940 along with BQ78350-R1 in our design, our BMS requires to operate at high Charge and Discharge Currents, but the BQ78350-R1 is allowing to set OCD to 30A max where as we need to operate up to 500A Max will the current sensor in AFE supports the current rate or should we change for external current sensor.
if AFE BQ76940 supports should we do any changes in the configuration of the Companion Controller BQ78350-R1
Kindly Suggest