This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51285A: TPS51285A 3.3V Output support

Part Number: TPS51285A

Dear TI Experts,

Greetings,

I have few questions regarding the operation of the TPS51285A. 

1. I just want only 3.3V output which is Channel 2 output so I am just giving 3.3V to EN2 pin. Will it work? Does it have any dependency on the EN1 pin or CH1 Circuitary?

2. What is function of VO1 pin of the IC?

3. Can I connect Simple RC delay to EN2 Pin which is derived from VREG3. which can give delay between VREG3 and 3.3V Out (Ch2)?

Kindly, Help in issue.

Thanks and Regards

Saunak Bhalsod