Hello,
I am currently working on a project utilizing the BQ40Z60 and we have noticed that the battery manager will not increment the cycle counter if our system is shut down and the manager is set to shutdown mode for some duration, before turning the system back on and waking the manager to normal mode to continue the cycle. This seemingly resets its progress of the cycle and as such if the manager enters shutdown mode often enough the cycle counter will never increment regardless of how many times the battery is discharged.
This has made us look at State of Health and Full Charge Capacity to help keep track of our cells. But the persistence of these values in relation to shutdown mode are not clear to us from the data sheet and reference manual, and testing them is much more difficult than the cycle counter. So we would like to ask if there is any list that could be made available on which data and statuses of the battery manager are affected by, or lost, if shutdown mode is entered. Or in the case that this is not available, if you could help us find out if State of Health and Full Charge Capacity specifically are determined in ways that are unaffected by the manager entering shutdown mode partway through a discharge cycle.
Best regards,
Andreas