Other Parts Discussed in Thread: TEST
Hi Sir,
My Customer is looking for a solution with below requirement and need the efficiency to be higher than 94% at 3A~4.5A.
Vin TYP= 12V, VIN=6~18V
Vout=7V, IOUT=3~4.5A
i think the LM34936-Q1 should be a good fit for this and I did a Webench simulation for them.
But Customer is asking if we have a EVM test result with same condition and automotive grade BOM?
May I know if you could help to advise if we have this kind of information or if you could run a bench test for customer?
The main reason that customer ask this is because the competitor are providing those data(layout/efficiency/thermal image) to them.
Thanks,
Patrick