Other Parts Discussed in Thread: LMZM33606, LMR33630
I am using LMZM33603 to generate a 9V DC rail from a 12V-24V input. Table 1 says the required Cout max for a 9V Vout is 110 uF. My 9V rail provides power to a processor board that has over 800 uF of capacitance on that rail. What will the effect be on the LMZM33603 if the output capacitance is way more than the recommended max from table 1?
What are my options for providing a 9V rail to this processor board? Should I consider a different DC/DC converter?