This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25600C: Standalone mode in Parallel operation

Part Number: BQ25600C


Hi,

Does this device work without host management even at the time in Dual Charger Operation?

Regards,
PAN-M

  • Pan-m,

    The bq25600C is a host controlled charger, but it can operate in default mode without host management. Please check if the default settings fit your application.

    Thanks,

    Ning.

  • Hi Ning,

    Also the dual mode, can this charger work without host management?
    Naturally I think the default to be usable.
    This device can be used as an autonomous charger with no host or while host is in sleep mode.
    And even a dual mode becomes the same setting because it is a default mode then.
    Therefore, Dual mode = Default mode = Standalone.
    Is this correct?

    Regards,
    PAN-M

  • PAN-M,

    The BQ25600C may operate without host as parallel charger. Since it does not support battery thermistor connection, it is not recommended to use as master charger or standalone charger.

    Thanks,

    Ning.